Menu
Menu
Menu

BLOG

February 17, 2023

Standard vs. Safety PLCs, which is better?

In the world of automation, there are many choices, and when efficiency and safety are on the line, making the right decision is critical. Motion Ai can help you make the correct choice based on […]
February 8, 2023

Open loop vs. closed loop: which system is better?

Open loop vs. closed loop: which system is better? Open loop vs. closed loop, which control system would benefit your operation more? It may seem like a tricky question at first, but after learning the […]
January 5, 2023

Why should you utilize CODESYS?

CODESYS stands for controller development system. While some may appreciate a good acronym, knowing what CODESYS stands for does not indicate what it is or why automation systems designers should employ it. What Does CODESYS […]
May 16, 2022

Why choose a PLC-Based Control System?

Programmable logic controllers (PLC) allow for the handling of programming languages for motion control in automation systems. These PLC-based control  systems continuously monitor input devices and automatically make decisions based on custom programming and logic, allowing them […]