Menu
Menu
✕
April 30, 2024

Quality Assurance in Automotive Manufacturing: Final Assembly Transmission Inspection

At its core, the Final Assembly Transmission Inspection system is designed to verify the presence or absence of 47 discrete components or objects within each transmission assembly. This system's ability to perform comprehensive inspections in less than 3 seconds, including the acquisition cycle, makes this system remarkable. This efficiency is critical in maintaining the flow of the production line without compromising on the thoroughness of the inspection.  
April 29, 2024

Copper Fitting Vision Inspection

The Copper Fitting Vision Inspection machine is not just any quality assurance tool; it's a comprehensive solution designed to uphold the highest quality standards in press-fit copper fittings. This state-of-the-art system thoroughly verifies part geometry, ensuring each component meets the precise specifications required for flawless functioning. The system also validates the placement and seating of O-rings within the fittings, a critical factor for ensuring leak-proof installations that stand the test of time.
April 29, 2024

Transforming the Inspection of Carbon Tubes

The inspection process is as crucial as production in manufacturing, especially when dealing with delicate materials like carbon honeycomb tubes. These components, known for their lightweight yet strong structure, are pivotal in various industries, including aerospace, automotive, and construction.