The Changes Automation is Making in the Textile Industry
March 7, 2023
Bin-Picking Solutions: A New Take on Old Processes
March 22, 2023
Artificial intelligence (AI) has caused waves since becoming mainstream in technology, along with other revolutionary changes. One major advancement is machine vision in logistics chains. The use of machine vision in warehouses is vast and always changing. From tracking shipments to scanning multiple barcodes, machine vision offers more potential than can be imagined in industries today.
The Beginnings of Machine Vision
In short, machine vision is the ability of computers to see. Machine vision uses hardware and software to identify codes or labels and make rapid decisions based on those labels. Common uses for machine vision are inspecting products, detecting defects, tracking products, and sorting packages.
Companies worldwide have been using early versions of machine vision since the 1970s. Originally machine vision was used in distribution houses as slug codes. They were the code used to sort the packages or products companies used for inventory. The major advantage was that a driver delivered a truck full of inventory to different stores and didn’t have to empty the entire truck looking for specific boxes. Instead, they were able to use the slug codes and make the entire process more efficient for everyone, saving time and money like never before.
Why You Should Use Machine Vision in Logistics
Machine vision has changed the face of logistics chains with multiple ways to be included in a facility for a more efficient environment. The logistics chain process includes the ease of shipping, sorting and producing products, quality checks, innovation, and accuracy. Utilizing machine vision makes shipping and sorting nearly 100% accurate – a huge step from where industry has been in the past.
Mistakes cost money, reputation, revenue, and relationships, but with the improved accuracy of machine vision, errors are close to none. Although these machines are not perfect, the improvement is inarguable compared to the statistics before the implementation of machine vision.
Benefits of Implementing Machine Vision
Warehouses have benefited the most from machine vision because of the multiple processes they take on day to day. Automation has allowed facilities to increase productivity, which in turn will bring in higher profits.
However, machine vision is not only applied to warehouses, but any logistics chain. AI is an excellent advantage for any machine-vision-driven facility.
AI has been the driving force for automation in almost every industry. With AI and machine vision, the logistics chain has turned around completely. Logistics chains that were once slow and unreliable have quickly become highly efficient and accurate systems. Not only is this a plus for companies worldwide, but it is a huge bonus for customers who rely on these companies for their services.
The Use of Machine Vision
The upgrading of commercial technology is more prevalent now than ever. Companies that have integrated robotics and machine vision are experiencing proven results through their investment. For example, other new technologies increase accuracy in sorting items based on dimensions, SKUs, and labeling.
Machine vision systems are being innovated every day and will only improve over time. The benefits of implementing machine vision systems have let companies alter how they fulfill orders and have increased profits altogether. There is no question that these systems will become widespread and readily accepted because of the results seen on the corporate bottom line.
Contact the team at Motion Automation Intelligence to learn more.