Don’t Make These Mistakes with Cobots
April 12, 2023
Machine Vision for Factory Automation
May 9, 2023
Machine and motion control has become increasingly vital in manufacturing and distribution centers worldwide. These tools have enabled the full automation of manual processes, increasing uptime, revenue, production, and more.
What Exactly Is Machine and Motion Control?
In simple terms, machine and motion control do precisely what they suggest: control motion and machines. Think of it like human anatomy; the motion controller is the machine's brain giving directions to different parts to function seamlessly and complete tasks. The actuator can be compared to the muscles or joints, enabling the machine to move and do specific tasks. Finally, the sensors are similar to our senses; they can detect temperature, vibration, currents, etc.
Machine and motion control is vital in the packaging, printing, textile, semiconductor production, and assembly industries. Automating manual processes has been a game changer for increasing profits and uptime. Implementing these devices has greatly reduced workplace injuries, costly mistakes, and time spent on processes.
Why You Should Implement Machine and Motion Control
Facilities everywhere are reaping the benefits of implementing machine and motion control. Utilizing these machines gives you time to focus on other tasks more critical than watching over the factory floor. Packaging is one area that has seen a drastic change after installing machine and motion control processes. Instead of manual labor prioritizing mundane tasks, employees can oversee machines and work on other tasks that robots cannot necessarily do.
No one likes mistakes, especially when they cost money, reputation, or revenue. Implementing machine and motion control prevents these missteps from occurring, saving your business in the long run. The numbers don't lie; after enforcing machine and motion control, revenue is higher, uptime is increased, and the overall happiness of employees is improved. There's no denying what machine and motion control can do for you.
Examples of the Benefits of Machine and Motion Control
Semiconductor production has thrived with the introduction of machine and motion control. Because the process requires extreme precision, these automated processes in microscopic situations have proven vital to success.
Along the same lines, the textile industry has heavily included machine and motion control for quick production. Textiles have seen an enormous increase in demand over the years, so implementing machine and motion control is critical to accurately keeping up with orders and requests.
Fully automating has been the goal for facilities everywhere, but partially automating your facility with machine and motion control could also unveil the same advantages. For example, textile production combines automation with manual labor, with benefits such as higher-quality items, quicker turnaround time, and ensuring employees' skilled maintenance of automation machines.
Stay Competitive With Machine and Motion Control
Upgrading technology with machine and motion control is quickly moving from an option to an informed business choice to stay competitive. Constant updates to different technology and processes are essential to keep up with demand and improve business performance.
Stay in the game and automate with machine and motion control today. You will see immediate results and thrive with your newly automated facility.
Contact Motion Automation Intelligence to learn more.