Menu
Menu
✕

BLOG

April 30, 2024

Quality Assurance in Automotive Manufacturing: Final Assembly Transmission Inspection

At its core, the Final Assembly Transmission Inspection system is designed to verify the presence or absence of 47 discrete components or objects within each transmission assembly. This system's ability to perform comprehensive inspections in less than 3 seconds, including the acquisition cycle, makes this system remarkable. This efficiency is critical in maintaining the flow of the production line without compromising on the thoroughness of the inspection.  
April 30, 2024

EBC Pump Filter Application

At the core of this revolutionary application is the use of SCARA robots, renowned for their speed and precision in part handling. This innovative approach allows for seamless and rapid inspection processes crucial in high-volume production environments. Complementing the robotic technology are two types of cameras: a line scan and an area scan camera. Together, they perform comprehensive inspections within a mere 1.2 seconds for each part, showcasing an impressive blend of speed and thoroughness.
April 30, 2024

Quality Control in Pet Food Manufacturing: The Automated Dog Treat Vision Inspection System  

his standalone system is designed to handle high volumes of dog treats. It has a buffer area for loading bulk parts, an infeed conveyor system to guide the treats through the inspection station and reject bins to segregate defective treats. After inspection, outfeed conveyors route the sorted, high-quality treats to their collection bins. The system can inspect 200 dog treats per minute, making it a high-speed solution tailored to modern pet food manufacturing demands.  
April 29, 2024

Plastic Syringe Vision Inspection

One critical area where technology is making a remarkable impact is in the inspection of syringes, a process crucial for ensuring the safety and efficacy of injections. Enter the high-speed syringe inspection system, a groundbreaking solution designed to elevate the quality control standards in syringe manufacturing.  
April 29, 2024

The Power of Inkjet Label Inspection Systems

One of the standout features of this system is its user-friendly interface. It displays statistical data of the inspection results, including part images and pass/fail criteria. This feature is particularly beneficial as it allows for modifying tolerances based on real-time feedback, ensuring that the quality of prints remains consistently high.
April 29, 2024

Copper Fitting Vision Inspection

The Copper Fitting Vision Inspection machine is not just any quality assurance tool; it's a comprehensive solution designed to uphold the highest quality standards in press-fit copper fittings. This state-of-the-art system thoroughly verifies part geometry, ensuring each component meets the precise specifications required for flawless functioning. The system also validates the placement and seating of O-rings within the fittings, a critical factor for ensuring leak-proof installations that stand the test of time.
April 29, 2024

Transforming the Inspection of Carbon Tubes

The inspection process is as crucial as production in manufacturing, especially when dealing with delicate materials like carbon honeycomb tubes. These components, known for their lightweight yet strong structure, are pivotal in various industries, including aerospace, automotive, and construction.